Other Parts Discussed in Thread: LAUNCHXL-F280039C, DRV8353
Hi Team
the DRV8353RS-EVM mention it's
"FOR USE ONLY WITH TI ISO-F28027F”
so this board can be only used for ISO-F28027F? or it can work with LAUNCHXL-F280039C

BRs
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team
the DRV8353RS-EVM mention it's
"FOR USE ONLY WITH TI ISO-F28027F”
so this board can be only used for ISO-F28027F? or it can work with LAUNCHXL-F280039C

BRs
Brian
Hi Brian,
Thank you for your question!
That understanding is correct, as the specific software GPIO pin mapping for the LAUNCH-F280027F is different from the LAUNCH-F280039C, and so the jumper configuration for inputs, ADCs, and outputs necessary to drive the DRV8353 most likely will not match.
It may be possible to jumper over the appropriate pins from the 39C to the EVM, but the base code/GUI is not designed with the board in mind.
Hope this information has been helpful.
Best Regards,
-Joshua