Part Number: DRV8353
Other Parts Discussed in Thread: MSP430F5132,
Tool/software:
Hi,
I am currently working on building a motor controller to drive 72V 3kW BLDC motor, I am following TIDA 00774 reference design for my goal.and considering to use DRV8353SRTAT (as it can drive up to 102V) component to drive MOSFETs. I want to ask several things about the component and general design of a motor controller.
1. Is it possible to use INHA, INLA, ... pins by just connecting to the MCU (MSP430F5132) without connecting them to HALL sensors. (because the competition that we are currently preparing for does not allow us to use automatic HALL commutation, as it will not counted as domestic product).
2. Do you suggest using only 6 MOSFETs (IPB044N15N5), or should I do MOSFET paralleling?
3. Can I use parallel MOSFETs with this smart gate driver (24 pieces of IRFP260-N)? Should I use external components (resistors, capacitors) for each of them if I ve done Mosfet parallelling? (Because the video about DRV8353 tells that it stores external components up to 24).
Please inform me on my design, what shouldn't I miss out, what specifically I should change to fabricate a controller that will work properly for my BLDC motor. I am also thankful that you share reference designs and documents like "Best Practices for Board Layout of Motor Drivers", and "System Design Considerations for High-Power Motor Driver Applications".
I have created schematics, but I have concerns over it, that's why I can start for PCB design.
Regards,
Mert
Koç University
Turkey