Tool/software:
Hi, I installed DRV8213-14-34EVM-GUI on windows and the first time I was able to connect to DRV8234EVM dev board. However, after disconnecting the usb and reconnecting I cannot connect to the serial port:
I don't know what else to try. When I connect the board the leds flash for some time (MCU_STATUS and GUI_STATUS) and I can see that two new COM ports appear on the computer (COM9 and COM15). But none of them work when I try to connect to them via the app