This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8262-Q1: Do I get four channel H-bridge motor driver for seat control?

Part Number: DRV8262-Q1
Other Parts Discussed in Thread: DRV8714-Q1

Tool/software:

Hi Reader,

Can anyone suggest me, where do I get four channel h bridge gate driver to connect three motors (single motor stalling current: 15A) with one h-bridge in common?

  • Hi Nihal,

    The DRV8714-Q1 is an automotive multi-Channel smart half-bridge gate drivers with wide common mode inline current sense amplifiers. It has two full H-bridges (4-channels or outputs) that can be controlled with Independent 1/2-Bridge, PH/EN, PWM modes. Independent 1/2-Bridge control will allow one H-bridge (in common) to drive a brushed-dc motor bi-directionally and the other two outputs can drive motors in one direction. 

    DRV8714-Q1

    Best,

    David