Part Number: DRV8412
Tool/software:
I am using a microcontroller with 0 to 3.3V digital outputs to control the PWMA-D lines on the DRV8412. I noticed in the DRV8412 datasheet that the maximum high-level input voltage is 3.6V. Does this mean that 3.3V may not be a high enough input voltage for the DRV8412 to register it as logic high? Am I reading this incorrectly?