Part Number: MCF8316AEVM
Other Parts Discussed in Thread: MCT8315EVM, MCF8315EVM
Tool/software:
I am working with a custom with the following specifications:
- 4 poles
- Resistance: 3.4 Ohms
- Inductance: 40 uH
- BEMF Constant: 10 mV/Hz
- Rated current: 500 mA
- Max RPM: 30k (1kHz)
- VM voltage 14V
The speed loop constants are unknown, and the motor comes with a load that I cannot remove for testing. I am currently using these values:
- Kp: 2
- Ki: 0.01
It starts with IPD and Slow Cycle, and not with align or double align.
With the present configuration (attached) it starts to spin and goes to open loop, then it ramps up the speed until it tries to get to close loop but always fails and stops spinning. Also, while it is in open loop it draws the maximum current according to the settings. Neither it seems like it is running smoothly in that mode, it's quite noisy.
I've tried with Enable Auto Handoff and without it, with different Minimum BEMF, with similar results. I've also disabled ABN_BEMF fault, which was activated each time it moved to closed loop. MPET has not worked. The same motor runs perfectly with MCT8315EVM.
{
"signature":"oneui-register-data",
"data":[
[
{
"idx":0,
"id":"ISD_CONFIG",
"value":"0x44E38CA0",
"addr":"0x00000080"
},
{
"idx":1,
"id":"REV_DRIVE_CONFIG",
"value":"0x283AF064",
"addr":"0x00000082"
},
{
"idx":2,
"id":"MOTOR_STARTUP1",
"value":"0x4B6941D0",
"addr":"0x00000084"
},
{
"idx":3,
"id":"MOTOR_STARTUP2",
"value":"0x11866002",
"addr":"0x00000086"
},
{
"idx":4,
"id":"CLOSED_LOOP1",
"value":"0x070381B0",
"addr":"0x00000088"
},
{
"idx":5,
"id":"CLOSED_LOOP2",
"value":"0x1AADCB19",
"addr":"0x0000008A"
},
{
"idx":6,
"id":"CLOSED_LOOP3",
"value":"0x1BA82B21",
"addr":"0x0000008C"
},
{
"idx":7,
"id":"CLOSED_LOOP4",
"value":"0x48D91770",
"addr":"0x0000008E"
},
{
"idx":8,
"id":"SPEED_PROFILES1",
"value":"0x00000000",
"addr":"0x00000094"
},
{
"idx":9,
"id":"SPEED_PROFILES2",
"value":"0x00000000",
"addr":"0x00000096"
},
{
"idx":10,
"id":"SPEED_PROFILES3",
"value":"0x00000000",
"addr":"0x00000098"
},
{
"idx":11,
"id":"SPEED_PROFILES4",
"value":"0x00000000",
"addr":"0x0000009A"
},
{
"idx":12,
"id":"SPEED_PROFILES5",
"value":"0x00000000",
"addr":"0x0000009C"
},
{
"idx":13,
"id":"SPEED_PROFILES6",
"value":"0x00000000",
"addr":"0x0000009E"
}
],
[
{
"idx":0,
"id":"FAULT_CONFIG1",
"value":"0x17E80206",
"addr":"0x00000090"
},
{
"idx":1,
"id":"FAULT_CONFIG2",
"value":"0x54C00000",
"addr":"0x00000092"
}
],
[
{
"idx":0,
"id":"INT_ALGO_1",
"value":"0x0275687D",
"addr":"0x000000A0"
},
{
"idx":1,
"id":"INT_ALGO_2",
"value":"0x00000027",
"addr":"0x000000A2"
}
],
[
{
"idx":0,
"id":"PIN_CONFIG",
"value":"0x00000000",
"addr":"0x000000A4"
},
{
"idx":1,
"id":"DEVICE_CONFIG1",
"value":"0x00000000",
"addr":"0x000000A6"
},
{
"idx":2,
"id":"DEVICE_CONFIG2",
"value":"0x0000B000",
"addr":"0x000000A8"
},
{
"idx":3,
"id":"PERI_CONFIG1",
"value":"0x40000000",
"addr":"0x000000AA"
},
{
"idx":4,
"id":"GD_CONFIG1",
"value":"0x0C000100",
"addr":"0x000000AC"
},
{
"idx":5,
"id":"GD_CONFIG2",
"value":"0x00200000",
"addr":"0x000000AE"
}
],
[
{
"idx":0,
"id":"GATE_DRIVER_FAULT_STATUS",
"value":"0x00000000",
"addr":"0x000000E0"
},
{
"idx":1,
"id":"CONTROLLER_FAULT_STATUS",
"value":"0x00000000",
"addr":"0x000000E2"
}
],
[
{
"idx":0,
"id":"ALGO_STATUS",
"value":"0x00000000",
"addr":"0x000000E4"
},
{
"idx":1,
"id":"MTR_PARAMS",
"value":"0x00000000",
"addr":"0x000000E6"
},
{
"idx":2,
"id":"ALGO_STATUS_MPET",
"value":"0x0A000000",
"addr":"0x000000E8"
}
],
[
{
"idx":0,
"id":"ALGO_CTRL1",
"value":"0xAA500000",
"addr":"0x000000EA"
}
],
[
{
"idx":0,
"id":"ALGO_DEBUG1",
"value":"0x80000000",
"addr":"0x000000EC"
},
{
"idx":1,
"id":"ALGO_DEBUG2",
"value":"0x00000000",
"addr":"0x000000EE"
},
{
"idx":2,
"id":"CURRENT_PI",
"value":"0x000C130E",
"addr":"0x000000F0"
},
{
"idx":3,
"id":"SPEED_PI",
"value":"0x00000000",
"addr":"0x000000F2"
},
{
"idx":4,
"id":"DAC_1",
"value":"0x00000000",
"addr":"0x000000F4"
},
{
"idx":5,
"id":"DAC_2",
"value":"0x00000000",
"addr":"0x000000F6"
}
],
[
{
"idx":0,
"id":"ALGORITHM_STATE",
"value":"0x00000000",
"addr":"0x00000210"
},
{
"idx":1,
"id":"FG_SPEED_FDBK",
"value":"0x7FFFFFFF",
"addr":"0x00000216"
},
{
"idx":2,
"id":"BUS_CURRENT",
"value":"0x00000000",
"addr":"0x00000410"
},
{
"idx":3,
"id":"PHASE_CURRENT_A",
"value":"0x00000000",
"addr":"0x0000043E"
},
{
"idx":4,
"id":"PHASE_CURRENT_B",
"value":"0x00000000",
"addr":"0x00000440"
},
{
"idx":5,
"id":"PHASE_CURRENT_C",
"value":"0x00000000",
"addr":"0x00000442"
},
{
"idx":6,
"id":"CSA_GAIN_FEEDBACK",
"value":"0x00010000",
"addr":"0x00000466"
},
{
"idx":7,
"id":"VOLTAGE_GAIN_FEEDBACK",
"value":"0x00000002",
"addr":"0x00000476"
},
{
"idx":8,
"id":"VM_VOLTAGE",
"value":"0x01E60000",
"addr":"0x0000047A"
},
{
"idx":9,
"id":"PHASE_VOLTAGE_VA",
"value":"0x0000376C",
"addr":"0x0000047E"
},
{
"idx":10,
"id":"PHASE_VOLTAGE_VB",
"value":"0x0000376C",
"addr":"0x00000480"
},
{
"idx":11,
"id":"PHASE_VOLTAGE_VC",
"value":"0x0000A646",
"addr":"0x00000482"
},
{
"idx":12,
"id":"SIN_COMMUTATION_ANGLE",
"value":"0x00000000",
"addr":"0x000004BA"
},
{
"idx":13,
"id":"COS_COMMUTATION_ANGLE",
"value":"0x00000000",
"addr":"0x000004BC"
},
{
"idx":14,
"id":"IALPHA",
"value":"0x00000000",
"addr":"0x000004D4"
},
{
"idx":15,
"id":"IBETA",
"value":"0x00000000",
"addr":"0x000004D6"
},
{
"idx":16,
"id":"VALPHA",
"value":"0x00000000",
"addr":"0x000004D8"
},
{
"idx":17,
"id":"VBETA",
"value":"0x00000000",
"addr":"0x000004DA"
},
{
"idx":18,
"id":"ID",
"value":"0x00000000",
"addr":"0x000004E4"
},
{
"idx":19,
"id":"IQ",
"value":"0x00000000",
"addr":"0x000004E6"
},
{
"idx":20,
"id":"VD",
"value":"0x00000000",
"addr":"0x000004E8"
},
{
"idx":21,
"id":"VQ",
"value":"0x00000000",
"addr":"0x000004EA"
},
{
"idx":22,
"id":"IQ_REF_ROTOR_ALIGN",
"value":"0x00000000",
"addr":"0x00000524"
},
{
"idx":23,
"id":"SPEED_REF_OPEN_LOOP",
"value":"0x00000000",
"addr":"0x0000053A"
},
{
"idx":24,
"id":"IQ_REF_OPEN_LOOP",
"value":"0x00000000",
"addr":"0x00000548"
},
{
"idx":25,
"id":"SPEED_REF_CLOSED_LOOP",
"value":"0x00000000",
"addr":"0x000005CC"
},
{
"idx":26,
"id":"ID_REF_CLOSED_LOOP",
"value":"0x00000000",
"addr":"0x000005FC"
},
{
"idx":27,
"id":"IQ_REF_CLOSED_LOOP",
"value":"0x00000000",
"addr":"0x000005FE"
},
{
"idx":28,
"id":"ISD_STATE",
"value":"0x00000005",
"addr":"0x0000067A"
},
{
"idx":29,
"id":"ISD_SPEED",
"value":"0x5D7D3FEA",
"addr":"0x00000684"
},
{
"idx":30,
"id":"IPD_STATE",
"value":"0x0005000C",
"addr":"0x000006B8"
},
{
"idx":31,
"id":"IPD_ANGLE",
"value":"0x00000000",
"addr":"0x000006FC"
},
{
"idx":32,
"id":"ED",
"value":"0xFFFFF99B",
"addr":"0x00000742"
},
{
"idx":33,
"id":"EQ",
"value":"0xFFFFF45E",
"addr":"0x00000744"
},
{
"idx":34,
"id":"SPEED_FDBK",
"value":"0x00000000",
"addr":"0x00000752"
},
{
"idx":35,
"id":"THETA_EST",
"value":"0x2AAAAC80",
"addr":"0x00000756"
}
]
]
}