Other Parts Discussed in Thread: MCF8315EVM
Tool/software:
Currently
we are using MCF8315A driver to spin a BLDC blower.
We are using the default configuration in the tuning guide
Address Name | Address | Recommended |
ISD_CONFIG | 0x00000080 | 0x64738C20 |
REV_DRIVE_CONFIG | 0x00000082 | 0xA8200000 |
MOTOR_STARTUP1 | 0x00000084 | 0x0B6807D0 |
MOTOR_STARTUP2 | 0x00000086 | 0xA306600C |
CLOSED_LOOP1 | 0x00000088 | 0x0D3201B5 |
CLOSED_LOOP2 | 0x0000008A | 0x9BAD0000 |
CLOSED_LOOP3 | 0x0000008C | 0x00000000 |
CLOSED_LOOP4 | 0x0000008E | 0x00000000 |
SPEED_PROFILES1 | 0x00000094 | 0x00000000 |
SPEED_PROFILES2 | 0x00000096 | 0x00000000 |
SPEED_PROFILES3 | 0x00000098 | 0x00000000 |
SPEED_PROFILES4 | 0x0000009A | 0x00000000 |
SPEED_PROFILES5 | 0x0000009C | 0x00000000 |
SPEED_PROFILES6 | 0x0000009E | 0x00000000 |
ALGO_CTRL1 | 0x000000EA | 0x00000000 |
FAULT_CONFIG1 | 0x00000090 | 0xBEC80106 |
FAULT_CONFIG2 | 0x00000092 | 0xF0D00888 |
PIN_CONFIG | 0x000000A4 | 0x00000000 |
DEVICE_CONFIG1 | 0x000000A6 | 0x00000000 |
DEVICE_CONFIG2 | 0x000000A8 | 0x0000B000 |
PERI_CONFIG1 | 0x000000AA | 0xC1C01F00 |
GD_CONFIG1 | 0x000000AC | 0x9C450100 |
GD_CONFIG2 | 0x000000AE | 0x80200000 |
INT_ALGO_1 | 0x000000A0 | 0xA433407D |
INT_ALGO_2 | 0x000000A2 | 0x000001A7 |
MTR_PARAMS | 0x000000E6 | 0x00000000 |
we tried to spin to different motors, to no avail
the motor used is Boreasa C60S1-01-L3 and Micronel U65ML-024KT the datasheets are attached
Radial Blower – U65ML-024KT-5 | micronel
https://www.boreasa.com/C60S1.html
It's worth noting that the driver reports no faults even when removed the motor connection, it failed to report the NO MTR fault