This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8329A: High side current sensing with MCT8329A

Expert 1225 points
Part Number: MCT8329A


Tool/software:

Hello,

bacause of PCB layout it would be much easier for me to have current sense resistor at high side.

I don't see it in datasheet but I asume CM voltage on MCT current sense pins not allow to use it as high side sensing (Vbus is 25V)

Is there a simple solution to use high side shunt and connect it with 1/1V amplifier with high CM directly to MCT?

If yes can you suggest some part number?

Ideally this would be CSA part with 1/1 gain but can be at least some OpAmp.

Adam