Tool/software:
Hi!
I wish to use two DRV8145 as an H-bridge, driving a single phase BLDC at 36V 35A up to 150K RPM. I intend to set them up as per the datasheet (image below).
I intend to feed both half bridges with the same 125 kHz PWM signal to their "IN" ports. This signal will be at 125 KHz constantly and only vary the duty cycle.
For the "DRVOFF" pin I intend to feed them a 100-20 000 Hz signal at constant 50% duty, where one half bridge receives a complimentary signal of the other.
With this setup I imagine I can control the current with the 125 KHz varying duty cycle and by varying the frequency of the "DRVOFF" signal, the rotational speed.
So, my main question is if it would be acceptable to not have any deadtime on the "DRVOFF" signal? Wouldn't just the "worst case" be that the motor is tied to say VIN on both sides for a micro second?
Is this overall a good setup or am I mistaken about something? Thanks for any suggestion!