This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3245Q-Q1: DRV3245Q-Q1 vs. DRV8353F

Part Number: DRV3245Q-Q1
Other Parts Discussed in Thread: DRV8353F, DRV8162, CSD, CSD18514Q5A, CSD18543Q3A, CSD88539ND, CSD87502Q2

Tool/software:

Hi..

One of my customer is looking for the motor driver solution for 24V/5A BLDC. They are considering 2 options, 1st is DRV8353F & 2nd is DRV3245q-Q1. They want to udnerstand the differeneces between two devices & want to know which one is better & which one is suitable for their application of Valve control. They also want functional safety.

Pls. help with the inputs.

regards,

Mitesh