This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8214EVM: I added the Missing R12 (56KOHM) but VM readings in GUI are off by 60%. Also can't update GUI to 2.0.2 it seems always stuck at "update in progress"

Part Number: DRV8214EVM
Other Parts Discussed in Thread: DRV8214

Tool/software:

1.  I added the missing R12 56K ohm resistor, but the VM readings reported by the GUI 2.0.0 don't match up with that measured on the "VM" terminal. For 3V on VM testpoint, the GUI reports 1.8V  For 5.0V on VM the GUI repots 2.9V. so they are reporting about 60% of the actual voltage.   Is the resistor value TI gave wrong, or did they change the calculation in later versions of the GUI?

2.  I am using the latest DRV821x_DRV823x-EVM-GUI download on the TI website which unfortunately is still 2.0.0.  There are no direct download links to 2.0.2.  It then says an update is available (2.0.2), and I let it update but it never finishes, just says update in progress and I can't see any network I/O happening so I think the update code doesn't work.