This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2625EVM-CT: Help with Haptic Driver Software Settings

Part Number: DRV2625EVM-CT
Other Parts Discussed in Thread: DRV2625

Tool/software:

Hello, 

I am using the haptics driver (DRV2625) with the evaluation board (DRM2625EVM-CT) to get preliminary haptic vibration data. The problem that I am having it after the system is connected and I have successfully drove the haptics motor, I am not able to put sequences in a series or add any delay between the sequences. See the highlighted section in the photo attached. Any ideas how I can fix this problem? 

Example of my goal: strong click -> delay 6ms -> transition hum 1 -> delay 3ms -> soft fuzz 

Thanks all!!