DRV8242-Q1: Can't clear nFAULT

Part Number: DRV8242-Q1

Tool/software:

I’m having trouble getting the DRV8242S-Q1 to work. After power-on and I set nSLEEP high, nFAULT goes low.  Then I send the CLR_FLT command (0x80 to register 0x08), but I never see nFAULT go high.  Is there some special sequencing I should follow?  Does the state of DRVOFF (or other control lines) matter when sending CLR_FLT?

Also, in 7.5.2 of the datasheet, it says the two MSBs are 1 – is this always the case? So when I read the DEVICE_ID, should I ignore the two MSBs?