The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8316-Q1: Motor driver recommendation request

Part Number: DRV8316-Q1
Other Parts Discussed in Thread: DRV8328, DRV8320

Tool/software:

Hi TI Team,

The customer is looking for a BLDC motor driver with 12V three-phase control.

Output voltage: 12V or higher

Output current: 16A or higher

Please recommend the product.

  • Hey Cho,

    I recommend looking into DRV8320/3, or DRV8328/9 family of devices that are rated for 60V. These are external FET drivers so the current capability will depend on the FET driven by the customer.

    The application need higher current than our integrated FET drivers can support so I recommend our ext. Fet drivers.

    Best,

    Akshay