This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8262-Q1: DRV8262-Q1

Part Number: DRV8262-Q1
Other Parts Discussed in Thread: DRV8962-Q1,

Tool/software:

i found one ic for driving DC Motors or Stepper motors.
Part number:DRV8962-Q1  : 65 V, Four-channel Half-Bridge Driver with Current Sense Outputs for 24V and 48V Automotive Applications
can you send the application notes to drive DC Motor or Stepper Motor as per the production requirement. I mean i will use one ic to  drive dc motor or stepper motor.
Please send application circuits or any other details to start my project. 
Thank you for your support