Tool/software:
Hi,
My application requires an rms current of 8A and peak current of 23A almost similar to the evaluation board current ratings.
In the evaluation board for DRV8714 7mohm is chosen as the sense resistor. So should I also select 7mohm as the resistor?Is there any criteria for selecting the sense resistor.I have selected 1mohm with required power rating when 23A peak flows. Is it sufficient?
Regards,
Reshma