Tool/software:
I use the DRV8323RS and would like to know the minimum current flow in Vm.
Since in the datasheet there is only typical (10,5 mA) and maximum value (14 mA) given, i ask here whether there is more information about the minimum value.
Are the minimum values deviating much from the typical values in the datasheet or where are the dependencies?
Btw I am using 47nF 10% Capacitor between CPH and CPL. A 1µF 10% Capacitor is connected between DVDD and AGND, in case that is relevant.