Other Parts Discussed in Thread: DRV8353, UNIFLASH, MOTORWARE
Tool/software:
Hi team,
1) We purchased the DRV8353RS EVM package along with the ISO-F28027F(which came along with the package). Initially I have done changes in the IS0-F28027F to work stand-alone without the DRV8353RS EVM (mentioned in the DRV8353RH-EVM: ISO-F28027F in Isolation Mode - Motor drivers forum - Motor drivers - TI E2E support forums) to go-through the Code file from Motor ware . I was able to flash the program and set breakpoints in the CCS studio initially. After 20 to 30 debugging sessions, the error "Error - 1135, Debug Probe Reported an Error" occurred. After that, I was not able to debug the program from CCS and this error was seen continuously. I have checked the Switch connections (Boot switch settings set as 1-1-1) as mentioned in the Datasheet and they are fine. I can observe a mild heating in the FTDI Chip FT2232HQ in the ISO - F28027F. Is there any solution to Identify the issue?

2) I would also like to know if changing the FTDI chip could solve the issue as mentioned in this forum XDS100v2 - Error connection to the target: (error -1135 @ 0x0) - C2000 microcontrollers forum - C2000︎ microcontrollers - TI E2E support forums. In case of changing the FTDI chip, would it require separate FTDI programming from my side?
3) I could not find any links to purchase only the Controller board (ISO-F28027F) suitable for the DRV8353Rs EVM, but I could find LaunchXL- F28027F modules that are available. Will the LaunchXL- F28027F support the DRV8353RS EVM (I could change the connectors on the Launchpad that can plug in with DRV8353 EVM)?