This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8350: Gate hold off resistor becomes smaller

Part Number: DRV8350

Tool/software:

I am currently using DRV8350RS, and when I operate it, the gate hold off resistor becomes smaller (120kΩ).
Please tell me the cause of the gate hold off resistor failure.

The attached file is the circuit diagram.

The circuit configuration is as follows.
MOSFET: PSMN5R6-100BS
VDRAIN=48V
VM=12V
Idriven=300mA

Thank you in advance.

DRV8350RS.pdf