This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8833: DRV8833

Part Number: DRV8833
Other Parts Discussed in Thread: DRV8210, DRV8212, DRV8837

Tool/software:

Hello Team,

Is the DRV8833 Motor Driver Suitable for a 4V Planetary DC Gear Motor with the Following Characteristics:

  • No-load Current: 0.25A
  • Maximum Current: 1.15A

Regards,

K.Saravanan

  • Hello Saravanan,

    Is the DRV8833 Motor Driver Suitable for a 4V Planetary DC Gear Motor with the Following Characteristics:

    • No-load Current: 0.25A
    • Maximum Current: 1.15A

    The DRV8833 is a dual H-bridge BDC driver. It can operate down to 2.7 V and support up to 2 A momentary peak currents for single H-bridge. Based on this it should be able to support the described BDC motor. The bridges can be connected in parallel to double the drive capacity.

    Other single H-bridges that may be suitable are DRV8837, DRV8210, DRV8212. Thank you.

    Regards, Murugavel 

  • Subject: Increasing 4V DC Motor Speed with DRV8833

    Dear Muragavel,

    We have been testing a 4V DC Motor with the DRV8833 driver.

    • Current Configuration:

      • AIN1: High (3.3V)
      • AIN2: Low (0V)
      • BOUT1: 3.8V (VM - Battery Voltage)
      • BOUT2: 0V
    • Observations:

      • Scenario 1: 4V DC Motor + DRV8833 + 3.7V Battery - Nominal Speed
      • Scenario 2: 4V DC Motor + Reference Device (Unknown Driver IC) + 3.7V Battery - Higher Speed

    In both scenarios, the Motor and 3.7V Battery remain the same.

    We would greatly appreciate your suggestions on how to increase the motor speed in our setup (Scenario 1) using the DRV8833 driver.

    Sincerely,

    K. Saravanan.

  • Hi Saravanan,

    The DRV8833 is a simple driver. I do not see anything unusual in the way you were using it. I assume the DRV8833 breakout board does not have sense resistors and the AISEN and BISEN pins are directly connected to GND.

    Observations:

    • Scenario 1: 4V DC Motor + DRV8833 + 3.7V Battery - Nominal Speed
    • Scenario 2: 4V DC Motor + Reference Device (Unknown Driver IC) + 3.7V Battery - Higher Speed

    Could you please measure the voltage across the motor terminals with each of this drivers? Not sure if the reference device board had a voltage boost that could have higher speed. Any difference in voltages across the motor would mean reduced or increased speed. Thank you.

    Regards, Murugavel