Other Parts Discussed in Thread: DRV8262,
Tool/software:
I am in the process of designing a gate controller product that will control dual bidirectional BDC motors operating at 24V with a power rating of 250W. As part of this design, I am evaluating suitable integrated gate drivers to meet the performance and reliability requirements of the application.
After conducting an initial analysis, I found that the DRV8262 seems to align well with my requirements in terms of functionality and specifications. However, I would like to ensure that I am considering all viable options. Are there any alternative gate drivers that you would recommend, which are similar to or better than the DRV8262 for this type of application?
In addition, it would be very helpful if you could connect me with a supplier or an application engineer who can provide further insights and support for this project.