Part Number: DRV8262EVM
Other Parts Discussed in Thread: DRV8842
Tool/software:
Hi,
Currently evaluating the DRV8262EVM for a stepper motor application in PWM mode, in our application we adjust VREF dynamically depending on the load.
What I have noticed is whenever VREF goes to 0V or is set to 0V the driver uses the full scale current on the motor (5A IFS) I am wondering if this is correct or if I am doing something wrong
If i set the value slightly above 0V it works fine
I currently have the EVM connected to our own microcontroller, that was currently communicating with 2 DRV8842 motor drivers for the exact same application and worked great
Regards,
Visaacan