This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8876-Q1: Output transient protections

Part Number: DRV8876-Q1


Tool/software:

Are there any recommendations for protections on the outputs of the DRV8876-Q1 device?  TVS to clamp voltage transients?  Diode to clamp negative voltage swings?

I am using the driver in independent PWM output control mode with a low current load (<10mA), but I want to make sure the outputs are protected from any potential transient events.