Tool/software:
Hi Sirs
Question:
1. We input positive voltage PWM signal(0~3V3) to DRV2511 with PVDD 5V => Driver could amplitude normal output from 3V3 to 5V
2. As PVDD 6~18V => Driver will produce impluse waveform instead normal PWM waveform.
=> We confirm the power source to PVDD is abundant.
=> Could you help to solve this issue?
Condition:
1. Driver Ouput: No load
2. Our schematic could be shown as attached.(Follow DRV2511 EVM and Parts)
3. Set up
- FS0, FS1, FS2 = Low
- STANDBY = Low
- Gain = 20kohm to Gnd
- Reg = 1uF to Gnd