DRV8412: DRV8412 Datasheet Revision H changes

Part Number: DRV8412

Tool/software:

Hello,

Can i know the reason of this change ? : Changes from Revision G (July 2014) to Revision H (July 2024): Deleted values in 39 to 200 in Table 6-2 .

It's about the Programming-Resistor Values and OC Threshold.

Because it's impossible to calculate this value ourself ,its a non linear relationship and no formula is given.

And the ROCP_CBC OC programming resistor range in cycle-by-cycle current limit modes is still 24-200 kΩ

I thought i was going crazy because i had a 84kohm value in a design and can't find a relationship with this value and the new 4 values table. Hopefully someone posted a screenshoot of the old table somewhere in the forum.

Thanks!