This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8662: Can I directly drive VIN without cap couple by AC signal?

Part Number: DRV8662

Tool/software:

DRV8662.TSCrefer to attched file that is TINA schemaic. Is it OK?

  • Hey Allen, 

    Expect a response from our expert asap. They are currently unavailable.

    Regards,
    Ore.

  • The coupling caps before input are essentially DC blocking capacitors so that the amplifier is only amplifying the AC signals. These are used in the circuit to provide better amplifier performance (CMRR, PSRR, VOUTerror, etc...) as well as lower power consumed by the DRV8662. If your signal possibly include the DC signals, it is recommended to add the coupling cap.

    Your schematic looks good to me. 

    Best,

    Hailong 

  • Because input signal frequency=1~60Hz, coupling cap will cause signal distorted.
    Input signals are from MCU output. They are complementary PWM signals. Vp-p=6V, Vp+=3V, Vp-=-3V

    __  __   3V

    |  |  |

    |  |_|      -3V

  • You can try using larger capacitors to minimize the impact on the 1-60 Hz PWM input. 

    The DRV8662 sets the DC operating point for the input and may not be 0 volts. So not having the capacitor there gives concern that an input voltage not centered around the same DC voltage won't have the gain properly applied or could get offset on the output. So it is recommended to have the cap there.