Tool/software:
Dear all.
Hi. I'm Moon
I am currently working with the DRV8701P motor driver and have some inquiries regarding the maximum chopping current that can be achieved with this IC.
-
Based on my calculations, I have set I(CHOP) to approximately 10.78A, but I have observed that current chopping is not occurring, and the current is exceeding 20A. Could you please confirm the maximum chopping current for the DRV8701P? (I have confirmed that the chopping current occurs normally up to 8A.)
-
Additionally, I would like to set the chopping current to 15A. If this is not feasible with the DRV8701P, could you kindly recommend an alternative IC that can support this requirement?
I would greatly appreciate your guidance on this matter.
Thank you in advance for your support, and I look forward to your response
Best regards.
Moon.