Tool/software:
hello team:
I have a question as follows:
In DRV8876-Q1 'S specification,there is some recommended external components for the device,and the R_PMODE is in one of them.
However,when an turn to Section 7.3.2. I did not see the recommended value of R_PMODE.

so, if I want to set PMODE PIN to Logic High,what the pull up resistor could be recommended, on the other hand,if I want set the PMODE pin to logic low,what the pull down resistor could be recommended.
Is there any risk if I set the pullup resistor or pull down resistor to 0 ohm? Like as follows