Tool/software:
I am trying to use this chip in the mode were I can just read the TORQUE_COUNT voltage but am not seeing expected results
Setup:
1) STL_MODE =GND
2) STL_REP = GND
3) 1/8 step mode (M0,M1 high)
My motor current is set by a pot between DVDD, Vref, and Gnd (vref ~0.75V).
The torque count is <50 mV when stopped. the only exception is that when i first come out of sleep it is ~2.4V. If i then do a few single steps it <50 mV and stays there. While executing a turns it sometimes rises to about 60mV but always is back to near 0 when done. These results don't change if i force a stall.
I'll note though, that there is a somewhat flexible coupling between the shaft i can grip and the motor so maybe that is affecting the results. The motor R is ~4.5 Ohm so think i shouldn't need the 8x gain.
Is it expected for the toque count be near 0 when stopped? Why can't i ever observe a significant voltage at this pin? The above data was with 1/8 micro stepping but fullsteps were basically the same.