This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3255-Q1: 48V-350A and 96V-300A Motor Driver

Part Number: DRV3255-Q1
Other Parts Discussed in Thread: UCC27301A-Q1

Tool/software:

Hello,

For our Forklift Inverter Motor Controller project, which will have two variants: 48V-350A and 96V-300A, we are planning to drive multiple parallel-connected FETs using a gate driver IC.

The DRV3255-Q1 is suitable for our 48V system, but I believe it is not appropriate for the 96V system.

Is there a gate driver IC similar to the DRV3255-Q1 that is suitable for a 96V and 48V system?

Best regards,
Egemen