Other Parts Discussed in Thread: DRV8212, DRV8213, DRV8215, DRV8214
Tool/software:
Hello,
I am interested in using one of your DRV821X series components. Mainly, I am interested in the Evaluation Boards of the DRV8212, DRV8213 and DRV8215 components because of the features they offer.
Our application is based on the implementation of a obstruction detection system for motorized components (primarily using DC motors). To achieve this, we need a driver capable of characterizing and monitoring motors (current, position, speed, etc.), as well as transmitting this information to different MCUs. We have seen that the evaluation boards of this family allow the connection of dverse DC motors and support isolation between sections to communicate with an external MCU via I2C.
We would like to confirm this in order to proceed with acquiring the devices and begin testing.
I would appreciate if you could tell me which option would be the most suitable one for this application, confirming the feasibility of connecting an external MCU that may be from a manufacturer or supplier other than TI.
Thanks in advance.