I bought a hight voltage motor control and PFC kit from TI. There are a TMS320F28035 control card and a TMS320F28335 control card attached with the PFC kit. The TMSS320F28035 is code preload by TI and the motor can be controled. But when I load a 28335 demo project which is provided by TI, the control GUI can not be connected. Could you please tell me how to run the demo project of HVPM_Sensorless_2833x? Thanks!
The loaded souce code is in the following path.
C:\TI\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v1.6\HVPM_Sensorless_2833x