Other Parts Discussed in Thread: DRV8235,
Tool/software:
Hi team,
I facing different issues with TI motor driver chips. First i selected DRV8235 to drive A linear actuator 24V 3A. While controlling actuator movement the chip burned. Finally we found that chip is not suitable for our application(Even though the power rating of actuator is below the maximum caapcity of DRV8235).
So we selected DRV8256. No i facing an issue
All control pins and power pins are at correct voltage levels, but the output not activated. The drivers were working. I have 5 actuators in my pcb..
While I was working, one or two drivers had to work. Then, even though I tried to drive, drivers who weren't even there had to work.
current issue: all drive pins and voltage pins are ok, but ouput not activating.