Other Parts Discussed in Thread: AM2434,
Tool/software:
Hi Team,
I am using code ethernetip_adapter_generic_device_rgmii_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang from the SDK ind_comms_sdk_am243x_09_02_00_15 version in our custom board with AM2434.
That is working for EtherNET/IP application. Now I want to add motor control code also in the same application.
Is there any motor control firmware example for the drv3205-q1 in combination with the LP-AM2434? The DRV3205-Q1 Evaluation Module is compatible with Launchpad boards, as I understand to use this need to integrate SPI, GPIO, PWM. From SDK of AM2434 which example code I can use to start.
An example would be very nice, to start our new safety BLDC motor motion control development.