This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8329-Q1: DRV8329-Q1

Part Number: DRV8329-Q1


Tool/software:

Hi Team,

We are facing an issue with DRV8329AQRGFRQ1 related to Hardware fault.

We have checked and found out that the fault is related to GVDD/BST undervoltage.

 We observed GVDD voltage dips to 7.72 voltage whereas PVDD is 13.83V and AVDD is 3.3V both are constant as shown in waveform below (Red is GVDD, Purple is PVDD).

 Current combination of capacitors on BST = 1uF and GVDD = 10uF.

CPH and CPL is having 470nF capacitor.