Tool/software:
Hello TI Team,
I am using the DRV8874EVM connected to our motor with the specifications per below.
The EVM’s PMODE is configured to GND for PH/EN Control Mode, set up for single motor operation. The EVM board is powered by 24V. When I adjust the IN1 potentiometer, PWM signals begin, and the motor starts rotating.
I have observed a ringing signal occurring at the falling edge of the OUT1/OUT2 signal. This effect becomes particularly pronounced when the PWM duty cycle is set around 6.21%.
Kindly see below for the waveforms.
I tried removing R7 and replacing it with a 0-ohm resistor, but the ringing signal still persists.
Could you please advise on the possible causes for this ringing and recommend effective methods for its mitigation?
Motor Spec:
Waveforms:

Schematic: