This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2700EVM-HV500: Maximum Current Rating

Part Number: DRV2700EVM-HV500

I am driving a piezo actuator  HD-PAF1419 on 212 using DRV2700EVM-HV500. I wan to know what maximum current amplifier can produce whike operating on 212V. According to graph between maximum output voltage and load current in section 6.1, if we are driving the piezo actuator at approximately 212 V, the maximum output current appears to be around 5 mA. Am I interpreting right? I wanted to confirm maximum current deliver by amplifier on 212V. Also, is there any experiemnt that I acan perform to measure it.

Kindly help me that.