Part Number: MCF8315D
Hi team,
My customer would use additional switch for the 24Vcc on/off. ( for turn off the MCF8315D VCC manually/externally by MCU when they are needed. do not want to use sleep mode.)
But currently their schematic for 5V is not using FB_BK 5V but using 5V for their main MCU.
At this condition, they would like to turn off their 24Vcc and question is :
- do they also have to turn off the 5V rail for MCF8315D which is mostly related to pull ups(I2C, FG, nFAULT, etc)?
If there is no issue to stay 5V for MCF8315D side then they would like to turn it on when they turn off the 24Vcc.
I guided them to use FB_BK 5V but they would like to sustain their schematic on their current project due to the schedule.
Best regards,
Ernest