This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8323RS: Dual Motor Position Control with LaunchXL-F28069M and BoostXL-DRV8323RS

Part Number: BOOSTXL-DRV8323RS
Other Parts Discussed in Thread: LAUNCHXL-F28069M, , MOTORWARE, DRV8323

Hello,

I was wondering if it posible to to dual Motor Position Control with LaunchXL-F28069M and BoostXL-DRV8323RS. I am trying to run instaspin lab13f to accomplish this. I have already been able to run lab13b and the prerequiste labs doing single motor position control. I see that the DRV8323RS does have the dual motor hal files, ex: hal_2mtr.c. So, I am wondering if this setup is even possible. If so where could I find the 2mtr hal files for the DRV8323RS.

Any assistance would be greatly appreciated. Thanks!