Part Number: DRV8162
Other Parts Discussed in Thread: CSD18543Q3A,
Hi,
Referring to DRV8162LDGSR specifications, please see below queries.
As per design requirements, the Input is 5V 1.2KHz PWM, the only signal to drive HS & LS, and no other GPIO is available to clear the latched condition during fault.
- Can this device be used to drive high-side load?
- Does it use same VDS threshold for both HS and LS FETs with the resistor connected to VDSLVL pin? In case, different MOSFETs are used for HS & LS, which one shall be considered critical for OCP VDS monitoring?
- Using IDRIVE1 and IDRIVE2 pins resistor, same gate drive current applicable for both HS & LS MOSFET?
- How is the slew rate managed?
- If nDRVOFF pin is tied to 5V supply, will it impact on its operation?
- Can GVDD and GVDD_LS be tied together to 5V? WIll it work with 5V(+/-2%) which will be an LDO output in our application, since the operating min is 5V for GVDD, GVDD_LS?
- Kindly guide us on the latch reset strategy.
- In case INL/EN is tied to 5V in 1-pin PWM mode, how will the fault-clearing mechanism work? Latched fault recovery INH(IN) = Low & INL(EN) = Low for > tCLRFLT (Reference- Table 7-7)
Regards,
Prachi
So if the GVDD is above this value then it should not be an issue. Also I assume 5V gvdd is enough to fully enhance the MOSFET being used in your application.