Part Number: DRV2700EVM-HV500
Hello,
In the DRV2700EVM-HV500 you have choosen the mosfet BSS127 H6327XTSA2, could you please suggest to me an appropriate mosfet for a 800V application (I_out= 10mA).
Thank you for your support.
Part Number: DRV2700EVM-HV500
Hello,
In the DRV2700EVM-HV500 you have choosen the mosfet BSS127 H6327XTSA2, could you please suggest to me an appropriate mosfet for a 800V application (I_out= 10mA).
Thank you for your support.
Hi,
Our team will take a look at your questions and get back with further comments this week after the holiday on Monday.
Best regards,
-Ivan Salazar
Applications Engineer
Hi,
Yes thank you. Could you please also explain to me how you did the calculation of Rd drain res and Rs source res (in the EVM is Rd=R27+R22 and Rs= R4)
Thank you for your support.
Lesdey,
Usually we don't recommend other parties' components, but I do some quick search and some examples can be IXYS IXTA08N100D2 or STMicroelectronics STB10N95K3.
The source resistor Rs sets the current for the transistor that interacts with feedback pin. For a 3.3V or 5V input, a value of 2kohm to 10 kohm is common. You can keep the similar value to the EVM.
The drain resistors Rd limit the current through the MOSFET and define the gain of the modulation on the feedback pin. For 800V, you must increase these values relative to the 500V EVM to keep the current roughly the same. Increase value by ~60% vs 500V design.Ensure your resistors Rd are rated for the high voltage (800V). Standard 0805 resistors often only have a 150V-200V rating; you may need to use multiple resistors in series or specific high-voltage rated components.
Thank you for your answer.
From my side I used IPN95R3K7P7ATMA1 with the appropriate feedback net resistor calculation for 800 V, but my circuit couldn't exceed 600V, is it normal ?
It is normal for your circuit to be limited to a lower output voltage (600V instead of 800V), likely due to the voltage ratings of other components in the feedback or output stage, not the primary MOSFET itself. The IPN95R3K7P7ATMA1 MOSFET has a Drain-Source Voltage (Vdss) rating of 950V, so it is capable of handling an 800V output.
Hello,
I tried to change the diode but the output voltage is still the same, I observed that SW voltage can’t exceed 50V even I changed feedback net resistors !
Do you have already a reference design for 800V or 1000V output ?
Thank you very much for your support.
Lesdey, we don't have a reference design for 800V or 1000V output unfortunately.
So what is the next step to verify if you could help me please !
thank you for your support.

Hello,
Is the voltage dropping with a load attached or is there no load?
Have you already confirmed all components are rated for the high output voltage?
Regards,
Sydney Northcutt
Hello,
The voltage drop is without load.
Yes I used components with appropriate voltage rating !
Thank you for your support.
Hello,
Can you share the transformer you are using?
Regards,
Sydney Northcutt
Hello,
I'm using ATB322515-0110 the transformer used in the DRV2700EVM500HV.
Regards
Hi Lesdey,
We will review your updates and get back to you as soon as possible.
Please expect some delay during 02/16 holiday.
Best regards,
-Ivan Salazar
Applications Engineer