Hi,
I am doing some basic test on DRV8412EVM. I put both M1and M2 on high, M3 on low to operate under Mode 4. Only PWMA testpoint, GVDD, PVDD are connected to their conterparts. But no matter how I adjust PWM duty cycle(even from 0% to 100%), the motor doesn't change direction. Some questions:
1. Should I connect the GND corresponding to PWM to somewhere on the device, which finally connected to MOSFET source electrode.
2. When I connect PWM (not in use) to ground, which ground should be connected to?
3. I need 2 Full Bridge to operate two motors seperately. Under mode 4, only one PWM input is used to operate Half bridge A and B.During operation, how to turn off all mosfet when I want to stop the motor? Similar situation under mode 1&2.
4. After I disconnect all wires connected to DRV8412EVM, electrostatic potential PVDD was around 1.6v, one night later, it became to 1.2v. How did that happed? This happened not only one time, sometimes around 0.7v, sometimes around 3.6v. Very incredible.
Somebody please help me.
Fang