This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Confused about DRV8432 in parallel mode

Hi,

I'm planning to use the DRV8432 for controlling a DC motor with a maximum current of 12A. So I need to use he DRV8432 in pararell mode. But, after readind the post 'DRV8432DKD cycle-by-cycle current limit' (http://e2e.ti.com/support/applications/motor_drivers/f/38/t/133322.aspx?pi239031349=2), I'm quite confused. Can I control the motor with a PWM signal in PWM_A and GND in PWM_B? Because, in principle, that's the way to do it. But, if I have understood correctly what it is said in the post, controlling like that causes that the DRV8432 is stuck when the output hits CBC limit.

In pararell mode I can't use the OC latched mode and I need to have control over the maximum current. So, is the only way to control the motor to connect a PWM signal to one input and the complementary PWM signal to the other input? Can I have any problem if I do it this way?

That is, if I want to use the parallel mode and to have the cycle-by-cycle current limit working correctly, how have I to manage the inputs?

Thanks,

Fernando.