Other Parts Discussed in Thread: DRV8833, DRV8834
hi,
I am writing a linux device driver for stepper motor.I need to rotate stepper motor in both direction.I am able to rotate stepper motor in clockwise direction but when i am trying this in counterclock wise then it moving only in back and forth.
I am using DRV8833 motor driver to drive the stepper motor.
To rotate motor in clockwise direction, i am using this configuration:-
Pin A1 Pin A2 Pin B1 Pin B2
1 0 0 1 = 0x9
0 0 0 1 = 0x1
0 0 1 1 = 0x3
0 0 1 0 = 0x2
0 1 1 0 = 0x6
0 1 0 0 = 0x4
1 1 0 0 = 0xC
1 0 0 0 = 0x8
And for counter clock wise i am using exactly opposite of this: 0x8 , 0xC , 0x4 , 0x6 0x2 , 0x3 , 0x1 , 0x9
But the motor is not rotating in counter clock wise, it only just moving in back and forth.
So any one please help me out of this problem.
Regards
Vikram Singh Shekhawat