Dear Madam or Sir,
I use L293 as an buffer and level shifter from 5VDC to 24VDC on two of our boards and it works perfectly except for one thing: shorting any of the outputs to ground kills the chip! Could you suggest me a solution to this problem? I suppose there is a protection circuit that has to be added on the board to protect the output. If there is a device with similar function and shortcut protection embedded in chip, it can also be a solution to the problem.
Regards,
Milos Stankovic