Other Parts Discussed in Thread: DRV8302, DRV8412, CONTROLSUITE
Dear Friend,
- The project given in this EVM has used PID for Feedback Current. May we get more torque than open loop DC Motor Control?
 - What is the minimum speed of rotation for any PMDC Motor (e.g. 3000 RPM, 40 V DC Motor, Applied Excitation: 40 V DC, 5 A)?
 - How many MOSFETs are excited at a time for single full H-Bridge? Whether TI has used 4 quadrant PWM techniques or not? If Yes, then is it converted into 4-Quadrant in DRV8302 by selecting some particular Mode, by using Mode Selection pin?