ON THIS PART CAN I SET THIS PART UP TO OPERATE LIKE A CLASS D AMP
WHERE I WILL HAVE A REF VOLTAGE ON BOTH THE + AND - INPUTS PINS 6 AND 7
WITH A CAPACITOR LETS SAY 1 MFD TO PIN 6 THE + INPUT I APPLY A TRIANLGE WAVE AT 100 KHZ
AND WITH A SINEWAVE APPLIED TO THE - INPUT PIN 7 I SHOULD START TO SEE THE OUTPUT MODULATE AND AS I INCREASE THE SINEWAVE THE MODULATION INCREASES UNTIL O GET TO A GOOD LEVEL OF THE TRIANGLE WAVE TOO AVOID CLIPPING OF THE OUTPUT
DO YOU THINK THIS PART WILL WORK AS STATED
LET ME NO THANKS
WILLIE L. MCCAIN