Can the DRV8818EVM, be used with external command from FPGA , using its board connectors pins?
Is the STEP,ENABLE pins are input or output?
If positive can you explain how to do it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the DRV8818EVM, be used with external command from FPGA , using its board connectors pins?
Is the STEP,ENABLE pins are input or output?
If positive can you explain how to do it?
Hi Eli,
Yes, the DRV8818EVM can be used with external commands. To do so requires removing the resistors on the EVM R101 through R109. This isolates the microcontroller from the DRV8818, allowing external control. The external signals can then be connected at either the test points or J6
Please refer to the DRV8818EVM user guide for details.