Hi,
I'm building a quadcopter for a university project, and I'm using the LM3S811 as the flight controller. I want to use four DRV8332 three phase motor controllers to interface to the four brushless motors I have (AX 2308N 1100kv Brushless Micro Motors from www.hobbyking.com/hobbyking/store/uh_viewitem.asp?idproduct=5429).
The 811 will generate PWM outputs that will be input to the 8332. The motors each draw up to a maximum of 10A at a maximum of 11V. Since the 8332 can source up to 13A of continuous peak current, is this application reasonable?
I am also designing the PCB myself, so I also need to choose a voltage regulator. I will most likely be using a LiPo battery pack that can provide at least 12V of input to the 8332 (failing that, I would need eight AA batteries). Does the regulator need to be able to output at least 40A (10A each for four motors), or am I thinking about this incorrectly?
Can someone recommend a regulator I can use? Also, is there a recommended heatsink for the 8332?
The 811 has six PWM outputs. How do I output to all four motors independently?
Thanks for any help! I would greatly appreciate any advice.