Hi
Q1- I'm using a drv2605Levmct. In binary mode 6 ,7,8,how can I start it? I am just select the mode and push the button,but it didn't work well.
For example,in binary mode 6, I push B1 to begin life test,it woks well. Then I cut off the power and return to the mode, I push B2 or B3 or B4, the led on the button and "active" are on with no reaction,so I have to cut off power again. I want to change the voltage of the buzz, but it seems no way.
Mode 7 is the same situation. And in Mode 8, the four buttons are all with no reaction.
Do I miss some steps? Or is it the 2605Levm-ct's problem?
Q2- Please send me a latest source code. I have one but it seems that the code doesn't match the user's guide well. The description of each button is a little weird and not in accordance with the real function. And what's the biggest difference between drv2605Levm-ct and drv2605evm-ct in testing actuator?
Xiaofei Hu